Inspiriraj se i uči uz Daikin
Inspiriraj se Daikin dizalicama topline i istraži kako naša rješenja mogu transformirati tvoj dom
Obitelj Wezeman – Leiden
Lorem ipsum dolor sit amet, consectetur adipiscing elit, sed do eiusmod tempor incididunt ut labore et dolore magna aliqua.
Obitelj Wezeman – Leiden
Lorem ipsum dolor sit amet, consectetur adipiscing elit, sed do eiusmod tempor incididunt ut labore et dolore magna aliqua.
Više priča
Saznaj više
Udobno se smjesti, uživaj i saznaj više o našim rješenjima
Više informacija
You can get advice on which type of heat pump is best suited to your home from a Daikin installer, staff at the manufacturer’s flagship store, or consult our residential solutions navigator.
Most heat pumps usually come with an indoor and an outdoor unit. Each unit produces sound when in operation, this sound is generally measured in dBA and these levels range from a scale of 0 dBA to 140 dBA.
When looking at sound levels you will also see specifications given for sound power level and sound pressure level.
Sound power level is the sound level measured directly at the source.
Sound pressure level is the sound level measured at a specified distance (usually 1.5 - 2 metres) from the source.
The indoor units of Daikin heat pumps generally produce a sound pressure level of about 30dBA, which is comparable to the sound of a person whispering.
Outdoor units, since they come in a bigger variety of sizes, range in sound pressure levels between 40dBA and 62 dBA, which are comparable to the sounds of birds a chirping and people having a conversation respectively.
The typical lifespan of a heat pump is generally between 15 and 20 years, though this depends on a number of factors. For example, maintenance. Although heat pumps are a low-maintenance solution, an annual check-up by your installer or service partner will help maximise its lifespan.
Ne! Dodatno, naši klima-uređaji (poznati i kao „dizalica topline zrak-zrak”) mogu pomoći smanjiti simptome alergija. Daikin integrira više filtara u sve svoje klimatizacijske jedinice: titanske deodorizacijske filtre, srebrne filtre za alergene i flash streamere koji uklanjaju prašinu i hvataju bakterije. Uz pravilno održavanje klima uređaja i dokle god se oni redovito čiste, ti će filtri pružati čišći i zdraviji zrak.
What is the function of an air purifier?
An air purifier can remove pollutants, allergens, and other contaminants from the air. Using a combination of technologies such as electrostatic HEPA filters, activated carbon filters and ionisers, air purifiers help to capture and neutralise pollutants making the air you breathe considerably cleaner.
The 5 benefits of using an air purifier
There are many advantages of having an air purifier at home or in the office, including:
- Improving indoor air quality by removing pollutants such as dust, pollen, pet dander, mould spores and smoke from the air.
- Reducing allergies and asthma symptoms by removing allergens from the air.
- Reducing odours such as smoke, cooking odours and chemicals by using activated carbon filters and other purifying technologies.
- Improving sleep is one of the key benefits of an air purifier. It creates a cleaner and more comfortable sleeping environment by removing pollutants and allergens from the air.
- Creating a more comfortable and enjoyable living or working space by removing pollutants and allergens from the air.
Yes, heat pumps can connect to either old or new radiators.
If you already have radiators in your home, high-temperature heat pumps or hybrid heat pumps (if you’re replacing a gas boiler) can easily connect to them and use existing piping without the need to replace the radiators or carrying out additional works.
Postoje četiri glavna načina kako učinkoviti ventilacijski sustav može sniziti životne i kućanske troškove. Oni su sljedeći:
1) Energetske uštede: Sustav HRV (koji je najbolji način za uštedu troškova) pomaže pri uštedi energije. Prenosi toplinu iz izlazećeg zraka u svježi zrak tako da održi stabilnost temperature. Time se smanjuje potreba za grijanjem, a time i štede energetski troškovi.
2) Manja opterećenja grijanja i hlađenja: Izmjenom vanjskog zraka i uklanjanjem ustajalog unutarnjeg zraka ventilacijski sustav pomaže smanjiti opterećenja grijanja i hlađenja HVAC sustava. Zauzvrat, time se može produljiti vijek trajanja HVAC opreme. Naposljetku, time se štede troškovi održavanja.
3) Blaže alergije i astma: Sustav DUCO Centralized HRV uvelike pomaže ublažiti simptome alergija i astme uklanjanjem štetnih čestica iz zraka.
4) Niski troškovi održavanja: Sustav Duco odlikuje se niskim troškovima održavanja te je izrađen od visokokvalitetnih materijala i napredne tehnologije, što ga čini robusnim i dugovječnim.
Osjeti razliku koju nudi Daikin
Sve što trebaš znati o našim rješenjima, održivosti doma i načinima upravljanja klimom u svom domu
Želiš saznati više?