Skip to main content

Air conditioning is used for cooling, right? Well, yes, but that is only a small part of the story. 

Modern air conditioning systems are air-to-air heat pumps, which can also be used for heating. But how exactly does that work? And what are the advantages and disadvantages of air conditioning as heating? You can read it in this blog post.

Air conditioning as heating: the story of Julie and David

Julie and David bought a detached house built in the 1960s that they thoroughly renovated. Both the living areas and the bedrooms were originally heated with an electrical system. They replaced it with an energy-efficient and user-friendly air-to-air heat pump from Daikin. David: "The choice for an air-to-air heat pump was quickly made. On the one hand because of the exceptionally low power consumption. On the other hand because of the high level of comfort, such as the fast response time and the possibility to both heat and cool. Our rooms are warm within ten minutes in the winter. In the summer we can cool the rooms down in a few minutes.” To provide the heat pump with electricity, the couple also had solar panels installed on the roof. “Thanks to our solar panels, we have greatly reduced our energy costs for heating and cooling,” they say happily.  

Heating and cooling based on cool air 

The air conditioning systems that allow you to cool and heat are also called heat pumps. They transport heat from one environment to another using a coolant. Innovative air-to-air heat pumps are an environmentally friendly way to extract heat from the air. For example, in the summer you can use the air conditioning to cool the rooms in your house. The heat from inside is then discharged to the outside. In the winter, you reverse the process. The heat pump then extracts heat from the outside air – this is even possible at an outside temperature of -15°C – and then releases that heat to the inside air, in order to heat your home.  

The advantages of heating with air conditioning 

If you decide to buy air conditioning, you may want it to do more than just cool or heat the air. A modern air conditioning system creates a perfect indoor climate. The very best air conditioners even filter the air for unhealthy or irritating particles, such as pollen. Such an integrated system has many advantages: You can connect one outdoor unit to multiple indoor units. You then control each indoor unit separately, for an optimal temperature in each room. The compact heat pumps are easy to install. Even if you only have limited space in your home, it is possible to install one. The advanced inverter and heat pump technologies ensure optimal efficiency and maximum energy savings. You will quickly notice this in your wallet! The air conditioners are available in various models, such as wall or floor models. There is certainly a unit that fits seamlessly with your interior.  

The disadvantages of heating with air conditioning

 If you are renovating, you cannot connect an air-to-air heat pump to existing heat emission systems, such as radiators or underfloor heating. If  you want to keep them, you can combine them with an air-to-water heat pump. Also important: you can connect a maximum of five indoor units to one outdoor unit of an air-to-air heat pump. Do you want to cool and heat more rooms? Then consider a different heat pump system, such as an air-to-water heat pump.  

What does air conditioning with heating cost? 

The price of an air conditioner that can both cool and heat depends on many different factors, such as the number of indoor units, the type of indoor unit, the capacity, the options, etc. For a detailed quote, please contact an installer in your area. Tip: if you are renovating and have a heat pump installed, you may be eligible for a subsidy. 

Our most popular air-to-air heat pumps

Dostupne boje
Klima-uređaj
Dostupne boje
Klima-uređaj
Klima-uređaj

Usporedi modele (1)

Usporedi modele

Want to discover the full range of air-to-air heat pumps

Check out our full range and find the model best suiting your needs and interior

More information about air-to-air heat pumps

Find the answers to all the questions you might have about air-to-air heat pumps and how they can work for you

Unutarnja jedinica klima-uređaja dio je sustava klima-uređaja koji se nalazi unutar doma te ispuhuje klimatizirani zrak u prostor.

Izbor unutarnje jedinice klima-uređaja ovisi o tvojim specifičnim potrebama, ali važno je razumjeti kako cijeli sustav funkcionira. Postoje različiti sustavi klima-uređaja (poznati i kao „dizalica topline zrak-zrak”), a svaki od njih odlikuje se drukčijim karakteristikama. Jedna od najpopularnijih vrsta koja se upotrebljava u kućanstvima jest split sustav, koji je podijeljen na dvije jedinice: jednu unutarnju i jednu vanjsku. Tijekom zagrijavanja vanjska jedinica usisava vanjski zrak i prenosi ga u unutrašnjost putem unutarnje jedinice, a taj je postupak obrnut tijekom hlađenja.


Postoje tri vrste unutarnjih jedinica klima-uređaja:

Zidne jedinice

Modeli za zidnu ugradnju (Stylish, Ururu Sarara, Daikin Emura, Perfera,) dolaze u različitim veličinama i bojama kako bi se mogle uklopiti u svaki interijer.

Podne jedinice

Modeli podnih jedinica (Perfera Floor) kompaktni su klima-uređaji koji se besprijekorno uklapaju ispod prozorske klupčice ili u prostorije s ograničenom visinom.

Kanalne stropne jedinice

Kanalne stropne jedinice. Ako ne želiš vidljivu unutarnju jedinicu, kanalni klima-uređaj može se ugraditi u spuštene stropove ili lažne zidove.

Unutarnja jedinica klima-uređaja dio je sustava klima-uređaja koji se nalazi unutar doma te ispuhuje klimatizirani zrak u prostor.

Izbor unutarnje jedinice klima-uređaja ovisi o tvojim specifičnim potrebama, ali važno je razumjeti kako cijeli sustav funkcionira. Postoje različiti sustavi klima-uređaja (poznati i kao „dizalica topline zrak-zrak”), a svaki od njih odlikuje se drukčijim karakteristikama. Jedna od najpopularnijih vrsta koja se upotrebljava u kućanstvima jest split sustav, koji je podijeljen na dvije jedinice: jednu unutarnju i jednu vanjsku. Tijekom zagrijavanja vanjska jedinica usisava vanjski zrak i prenosi ga u unutrašnjost putem unutarnje jedinice, a taj je postupak obrnut tijekom hlađenja.


Postoje tri vrste unutarnjih jedinica klima-uređaja:

Zidne jedinice

Modeli za zidnu ugradnju (Stylish, Ururu Sarara, Daikin Emura, Perfera,) dolaze u različitim veličinama i bojama kako bi se mogle uklopiti u svaki interijer.

Podne jedinice

Modeli podnih jedinica (Perfera Floor) kompaktni su klima-uređaji koji se besprijekorno uklapaju ispod prozorske klupčice ili u prostorije s ograničenom visinom.

Kanalne stropne jedinice

Kanalne stropne jedinice. Ako ne želiš vidljivu unutarnju jedinicu, kanalni klima-uređaj može se ugraditi u spuštene stropove ili lažne zidove.

Da, a ako renoviraš svoju nekretninu i prijeđeš na obnovljivi klima-uređaj, dodat ćeš vrijednost svojem renoviranom domu, okolišu i svojem budžetu. Dizalice topline mogu se ugraditi u gotovo svaki dom. Međutim, postoje određeni aspekti koje je možda potrebno uzeti u obzir, posebice kada je riječ o izolaciji. Kako bi dizalica topline mogla najučinkovitije raditi, tvoj dom mora biti kvalitetno izoliran kako bi se u što većoj mjeri spriječio gubitak topline. Iskusni inženjer može te savjetovati što se u tvojem domu mora napraviti kako bi ispunio uvjete za sustav dizalice topline. Te mjere mogu uključivati nadogradnju izolacije zidova i krova. Također, u obzir se mora uzeti lokacija. Vanjska jedinica mora se ugraditi izvan tvojeg doma te nalaziti na mjestu gdje joj možeš jednostavno pristupiti kada je trebaš očistiti, prilagoditi njezine postavke ili servisirati dizalicu topline.

Da, klima-uređaj (poznat i kao „dizalica topline zrak-zrak”) može osigurati toplu vodu u tvojem domu. Uz Daikinovo rješenje Multi+ grijanje, hlađenje i topla voda isporučuju se putem jednog sustava. Povezuje se s do tri jedinice i jednim spremnikom tople potrošne vode te je kompatibilan sa spremnicima od 90 i 120 litara i cijelim nizom unutarnjih jedinica, čime nudi jedinstvenu fleksibilnost. Naše rješenje Multi+ uključuje intuitivan prikaz za nadzor i prilagodbu svih postavki, uključujući postavljanje rasporeda i temperature vode.

Daikin klima-uređaji (poznati i kao „dizalica topline zrak-zrak”) mogu ublažiti simptome alergija jer hvataju alergene i poboljšavaju kvalitetu zraka. Osim što griju i hlade, naši klima uređaji i uklanjaju zagađivače, pelud i čestice iz zraka.

Neke Daikin jedinice također su opremljene funkcijom „Flash Streamer” i različitim filtrima poput titan-apatitnog dezodorirajućeg filtra ili srebrnog filtra za uklanjanje alergena, koji mogu brzo i učinkovito smanjiti količinu zagađivača u zraku.

Ne! Dodatno, naši klima-uređaji (poznati i kao „dizalica topline zrak-zrak”) mogu pomoći smanjiti simptome alergija. Daikin integrira više filtara u sve svoje klimatizacijske jedinice: titanske deodorizacijske filtre, srebrne filtre za alergene i flash streamere koji uklanjaju prašinu i hvataju bakterije. Uz pravilno održavanje klima uređaja i dokle god se oni redovito čiste, ti će filtri pružati čišći i zdraviji zrak.

Kako bi tvoja dizalica topline mogla propisno funkcionirati, važno je da se sustav pravilno ugradi. Ugradnju na prikladnoj lokaciji morao bi provesti samo ovlašteni tehničar. Površina mora biti dovoljno čvrsta kako bi mogla podnjeti težinu i vibracije jedinice, a usto je potrebno osigurati dovoljno prostora za protok zraka te spojne cijevi i strujne kabele. Sve biljke ili grmlje koji se možda nalaze u blizini tvoje dizalice topline morali bi biti udaljeni najmanje jedan metar te ih se treba redovito podrezivati. Dizalica topline također bi se morala ugraditi na mjestu koje je jednostavno pristupačno za provedbu servisa i općenita održavanja.

Korisnici nas često pitaju zašto se dizalica topline ne može postaviti u zatvorenom prostoru. Ne bi li se mogao ugraditi u tavanskom prostoru ili zimskom vrtu? Odgovor na to pitanje glasi „ne”. Razlog je taj što bi dizalica topline nakon nekoliko sati izvukla svu toplinu iz zatvorenog zraka i praktički pretvorila taj prostor u hladnjaču. Zato je klima-uređaju potreban pristup slobodnom zraku na otvorenom.

Preporučujemo da servis jedanput godišnje obavi kvalificirani inženjer. Zakazani termini servisa, redovito održavanje, nasumične kontrole i rutinsko čišćenje sustava produljit će njegov vijek trajanja i očuvati energetsku učinkovitost.

Ovo su neke od naznaka da je tvojem klima-uređaju (poznat i kao „dizalice topline zrak-zrak”) odmah potrebno održavanje:

Ako tvoja jedinica klima-uređaja proizvodi više buke nego što je uobičajeno, možda su filtri začepljeni. Očisti jedinicu tako što ćeš prašinu ukloniti usisivačem. Ako se buka ne otkloni ili čuješ zvuk grgljanja, možda je u pitanju mehanički problem. U tomu slučaju pozovi stručnjaka da provjeri jedinicu.

Curious to learn all about air-to-air heat pumps?

Read the full story about air-to-air heat pumps and make an informed decision

Discover more home solutions

At Daikin, we believe that a house becomes a home through comfort, care, and the joy of shared moments. Discover our comfort solutions for your home.