Skip to main content

Naša mreža pouzdanih, kvalificiranih instalatera postavlja nova mjerila u pogledu profesionalnih i pouzdanih usluga ugradnje koje premašuju očekivanja kupaca

  • Visokokvalitetna ugradnja od strane educiranih stručnjaka
    Ikona muškarca
  • Naši su tehničari stručnjaci u pogledu svih relevantnih sigurnosnih pravila
    Ikona štita sa simbolom certifikacije
  • Nabavi Daikin dodatno jamstvo putem naših partnera
    Ikona Daikin jamstva

Pronađi instalatera

Naši pomno odabrani partneri posluju uz više od 45 godina inovacija i iskustva diljem Europe. Instalateri su naši najbolji ambasadori i s njima surađujemo kako bismo klimatizacijska rješenja učinili dostupnima svima.

Muškarac u uredu

Više informacija

Daikin works with trusted certified installers close to you. Go to our Technical Support page and use the interactive map to find your nearest installer. They will arrange a site visit to discuss your project and understand your needs, before suggesting the best solution for your home or place of work.

Yes, your certified installer is your primary contact for repairs. If they don’t offer repairs, you can contact the Daikin local office, which will give you a list of installers who can carry out repairs on your unit.

Yes. If your installer provides maintenance, you can continue using them for the maintenance of your unit.

The simplest answer is, it depends. Installing a heat pump is more than just the placement of an indoor and an outdoor unit, therefore there is no definite timeframe when it comes to the amount of time it will take to install a heat pump as it will depend on a number of different factors such as:

  • Type of home: The first thing that will be taken into account is the type of home a heat pump will be installed in. Is it a new-build or an existing home? With new-build homes, the planning needs to be taken into account with all other building currently taking place. With existing homes, things such as whether existing emitters will be used or will be replaced with new ones will play a part in the time needed.
  • Type of heat pump: Since there is a variety of different heat pumps, each one also has its own time requirement for the installation.
  • Additional works: Whether you are installing a heat pump in an existing or new-build home, there may be additional works that need to take place in order to ensure that you’re getting the most out of your new system. This could include the installation or replacement of emitters (such as radiators), optimising your insulation etc.
Par koji se smije na krevetu

Stand By Me certificirani partneri

Uz mrežu ovlaštenih servisnih partnera, Daikin Europe raspolaže vodećim znanjem i resursima na tržištu za stvaranje inovativnih rješenja za grijanje i klimatizaciju. Putem našeg Europskog razvojnog centra i uz fokus na energetsku učinkovitost stvaramo klimatizacijska rješenja za sve.